This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM339: issue with output goes low randomly

Part Number: LM339


Tool/software:

We've designed circuit using part number - LM339DRG3.

Circuit is used as basic comparator.

Multiple IC's are present on board with same part number and similar circuit.

Suddenly All IC's output goes low irrespecitve of input signal changes.

After Power restart of 5V supply all works normally again.

Please find below circuit diagram for reference.

  • Hello Akhil,

    1) Does any input go below (more negative than) -0.3V? ; Probably much below.

    2) Does the pull up voltage for all the outputs drop to 0V?

    3) Does the reference voltage of 160mV (V R72) go suddenly much higher?

    These are the only reasons that come to mind that would match your symptoms.

  • Hello Ron,

    At the time of the issue, I was not able to check the input because the PCB was not accessible without removing power.

    1) Does any input go below (more negative than) -0.3V? ; Probably much below.

    In a single system, we have around 100 sensor inputs, and it is highly unlikely that all of them would suddenly go wrong unless there is a problem with the 5V supply, as per my observation.

    2) Does the pull up voltage for all the outputs drop to 0V?

    Yes, all sensor outputs drop to zero suddenly and never recover, except after a power restart.

    3) Does the reference voltage of 160mV (V R72) go suddenly much higher?

    Not measured at the time of the issue, but there is a voltage divider, and 3.3V is perfect on the supply side, so this is unlikely.

    It seems like something is wrong with the 5V supply to the IC, which is causing this behavior.

  • Akhil,

    have around 100 sensor inputs, and it is highly unlikely that all of them would suddenly go wrong

    So many more than one LM339 stops working at same time. The 5V supply is the common item.  

    t seems like something is wrong with the 5V supply to the IC, which is causing this behavior.

    I agree.