Part Number: BUF802
Tool/software:
HI Experts,
For the BUF802, there are three bias pins R_bias, IN_Bias, and Aux_Bias. for R_bias there are plots of the bandwidth versus two bias points, and a plot of bias current vs R_bias pin resistance (pg 18 of the datasheet). The plot yields an equation of (7.83mA + 100(4.56/Rbias), and the bandwidth and IQ results are documented.
The voltage presented at IN_Bias and Aux_bias is not documented, so that a bias current can be calculated. In addition there is no documentation on how to choose a bias current, if the voltages were known?
IN bias current and IN_Aux bias currents are presented in the datasheet, but are not bipolar but positive only. Which direction is the current flowing for a positive bias current, into or out of the pin?
VOS, for IN, is presented in the datasheet, but is only negative. Since VOS is modeled as in series with the input signal, what 'direction' is it in series with the input signal? That is, is the voltage presented to the amplifer higher (more positive) or lower, by the VOS amount, than the voltage present at the pin?
The functional block diagram in Figure 8.1, shows DC voltages between the CLL, CLH and the bases of the corresponding clamp transistors. These DC voltages are not documented in the datasheet?
Regards,
Josel