Part Number: LMC6482
Tool/software:
In my application the amplifier mounted on PCB is powered in single supply mode 0V-10V, in buffer configuration

When IN+ is 10V the output is 9.55V. The output does not reach the positive rail.
Changing the input voltage from 0V to 10 V I obtained the following graph of Vout


As you can see if Vin excedees the value of 9.55V the output remains at 9.55V.
Why I can not reach the positive rail?
And how can I solve this problem?
Thanks in advance,
Emanuela