Other Parts Discussed in Thread: TL074, , TL074H, OPA4991-EP
Tool/software:
Hello Team,
Here is the analog output application with TL074QDREP in motor drive. The bias supply of TL074QDREP is 0V(VCC-) and 15V(VCC+). With this configuration and below circuitry, When pin10 is 0V, the output of TL074's pin8 is 12V. However, when VCC- pin is changed form (0V) to (-1V) and the VCC+ is 15V, with that dual bias power the OPA's output is normally. We are curious why it doesn't work with single bias power. Could you help to check on this issue! Thnak.s