Part Number: UCC28750
Other Parts Discussed in Thread: TINA-TI
Tool/software:
Hi,
I am planning to design an isolated 3-output, 3W flyback converter using the UCC28750. My input voltage range is either 10V to 60V or 10V to 48V.
Before proceeding with the design, I would like to simulate it using TINA-TI. However, I was unable to find a TINA model for the UCC28750. Could you please assist me in obtaining the simulation model?
Additionally, I would like to know if TI offers any alternative flyback regulator ICs that would suit my specific requirements.
Requirements:
- Input Voltage: 10V to 60V or 10V to 48V
- Output Voltages: 12V, 5V, and 48V (isolated from the primary side and isolated from each other)
- Output Power: 3W
- Efficiency: 70% to 80%
- Secondary-side Regulation: Required
Thank you for your assistance.