Part Number: THS4532
Other Parts Discussed in Thread: THS2630
Tool/software:
Hi team,
My customer's schematic is below. They want output offset as possible as equal to zero. Can some adjust method to improve? If change to THS2630, does the around component need to change? Thanks
Input signal 2.31 Vp-p
Input offset 1.65V
Pic2 is the output waveform as SIN and COSIN
Sin is red and Max=911mV min=-889mV
Cosin is green and Max=892mV min=-910mV