This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA4235: Accuracy issue in <5mA

Part Number: INA4235

Tool/software:

Hi team,

We occur TI INA423X GUI tool will configure wrong number in calibration parameter with max expected current 3A, so I calculate the right number and fill in (5107).

After that, I read the Current register to calculate the real current as below Table1.

 

As you see, the error will rise quickly under 5mA, even I read power for a while to calculate average current.

 

1mA/5mA measurement

Power value

Power(W)

BUS value

BUS volt

Current

Enegy value

Energy(J)

E=>Watt

E=>Current

2

0.0058594

2623

4.1968

0.001396

7272

21.30469

0.005918

0.00141011

8

0.0234375

2623

4.1968

0.005585

13736

40.24219

0.022357

0.0053271

 

 

Table1

CH1:10m ohm

VBUS:4.2V

Current Load

R_SHNT

max expect current

Current _LSB

SHNT_CAL

Current_REG

measured current

error(%)

3

0.01095

3

9.15527E-05

5107.219482

32,767

2.999908447

0.00

2

0.01095

3

9.15527E-05

5107.219482

21829

1.998504639

0.07

1

0.01095

3

9.15527E-05

5107.219482

10912

0.999023438

0.10

0.8

0.01095

3

9.15527E-05

5107.219482

8728

0.799072266

0.12

0.7

0.01095

3

9.15527E-05

5107.219482

7636

0.69909668

0.13

0.6

0.01095

3

9.15527E-05

5107.219482

6546

0.599304199

0.12

0.5

0.01095

3

9.15527E-05

5107.219482

5451

0.499053955

0.19

0.4

0.01095

3

9.15527E-05

5107.219482

4361

0.399261475

0.18

0.3

0.01095

3

9.15527E-05

5107.219482

3272

0.299560547

0.15

0.2

0.01095

3

9.15527E-05

5107.219482

2182

0.199768066

0.12

0.1

0.01095

3

9.15527E-05

5107.219482

1092

0.099975586

0.02

0.08

0.01095

3

9.15527E-05

5107.219482

875

0.080108643

-0.14

0.06

0.01095

3

9.15527E-05

5107.219482

658

0.060241699

-0.40

0.04

0.01095

3

9.15527E-05

5107.219482

439

0.04019165

-0.48

0.02

0.01095

3

9.15527E-05

5107.219482

222

0.020324707

-1.62

0.01

0.01095

3

9.15527E-05

5107.219482

110

0.010070801

-0.71

0.005

0.01095

3

9.15527E-05

5107.219482

55

0.0050354

-0.71

0.003

0.01095

3

9.15527E-05

5107.219482

35

0.003204346

-6.81

0.001

0.01095

3

9.15527E-05

5107.219482

12

0.001098633

-9.86

Thanks!

Jeff