Part Number: OPA990
Tool/software:
The datasheet of OPAx99 specify the power supplies of ±20 V or 2.7 V to 40 V.
I would like to use the amplifier:
- with an asymmetrical supply of +5 V and -25 V, and
- in the inverting amplifier configuration with the negative input pin within the recommended input voltage range and the positive input pin connected to 0 V.
I don't see any issue, but can TI please confirm that this asymmetric supply works with chip as well?
Thank you!