Hello, and thanks for reading!
I am working to implement a battery monitor for a hybrid vehicle as part of my senior design project. Our vehicle currently uses six 12V lead-acid cells (but that is subject to change), and I would like to read terminal voltage on each battery. My issue is that "ground" for the highest potential battery is actually at +60V relative to the ground of the lowest potential battery, so I can't have everything input to the same circuit directly.
I am looking at the ISO 120/121 isolation amplifiers to convert all battery voltages to a common ground so I can read them with an ADC, but I'm not sure what to make of all the connections on the IC. There is no functional pin description in the data sheet that I could find, and I'm not sure which of these pins are inputs, which are outputs, what I need to supply power to and which I can leave alone. The figures are only mildly helpful; there aren't any that definitively specify anything for this chip.
I'll post what I think are required, and please correct me where I'm wrong:
C1H/C1L , C2H,C2L ---> Clock speed capacitors. Set these to setup the IC for the band of external clock frequencies specified on page 7 of the data sheet.
Vin ---> The positive voltage I'm trying to read (+12V to the negative terminal of the battery, up to +72V relative to vehicle ground)
GND1/COM1 ---> Reference ground for the voltage I'm trying to read (the negative terminal, up to +60V relative to vehicle ground)
Vout ---> Isolated voltage output, equals Vin except it's now Vin relative to the vehicle ground (desired)
GND2/COM2 ---> Vehicle ground, the reference ground for Vout
I have no idea what +/- Vs1 is for (Figure 3 in the datasheet would have it appear to be an output (?) but I don't know what for)
Likewise, I have no idea what +/- Vs2 is, and I don't know if the external clock is required or optional.
Any help would be greatly appreciated.
Thanks,
Chuck Saunders
Veteran, USN