Part Number: LMV358
Tool/software:
Hello experts,
My customer is using LMV358 and had some questions regarding when the IC ambient temp is higher than ABS value,
1. When the ambient temp is over 150℃ for a while, what kind of issues may happen?
2. Would it matter if the IC is being powered or not when the ambient temp is higher than 150℃? In other words, if the IC were not powered and completely turned off, while ambient temp went over 150℃, would it have the same type of damage as if it were being powered?
3. If the ambient temp went over 150℃ then later was lowered to 50℃, and afterwards the IC operates normally, is it ok to keep using the IC? Or could it cause future problems?

Thank you in advance for your help and support.