Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

LT1014A: curve of the capacitive load

Part Number: LT1014A

Tool/software:

Hello Team,

My customer is requesting if we can provide the curve of the capacitive load according to overshoot for the device LT1014A.

Regards,

Renan

  • Renan,

    We would need to measure that curve as we currently do not have that.  Your customer could also measure this information, but Appling a 10mVpk square wave to the input of an op amp buffer with different capacitive loads.  The frequency setting for this measurement is normally between 1kHz to 100kHz and is adjusted as needed to make the waveform easy to read on the oscilloscope.  I do not have samples of this device, so doing this measurement will take some time (some time in Q1 of 2025).  I suggest having the customer measure this as it is a relatively simple test if you have parts on hand.

    best regards, Art