Part Number: AMC3302
Other Parts Discussed in Thread: THS4131, AMC3301,
Tool/software:
Hi,
I need to measure the current up to 50A.
50A x 1mOhm = 50mV
50A x 5mOhm = 250mV
AMC3301 and AMC3302 both are fulfilling the requirement. After this, we need to amplify the 2V output to 10V output. (using THS4131).
Could you please suggest the device suitable for the current sense requirement (AMC3301 or AMC3302).
Thanks & regards,
Ilamparithi Tamizhanangu.