Part Number: OPA328
Other Parts Discussed in Thread: TIDA-01055, REF35, OPA388
Tool/software:
Hello TI support,
We are going to use OPA328 for SAR reference buffer circuit. I gone through TI design, TIDA-01055 and document "Do-it-yourself: Three Ways to Stabilize Op Amp Capacitive Loads". I have attached the image of the circuit & below are some explanations,
1. I have used RISO+DFB+RFx as compensation method for 20uF output capacitor. The circuit is stable but closed BW is near 7.4KHz (-3dB).
2. SAR is designed to work on approx 2MSPS. So is it acceptable that reference buffer circuit with near 7.4KHz BW is sufficient for this application? provided reference may see transient at much higher frequency.
3. How wideband amplifier will play the role for such application with above mentioned BW.

Regards,
jagdish