Tool/software:
I am using the INA333 in a PT100 reader circuit and only need good performance near DC. Is it possible to limit the gain bandwidth of the INA333?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am using the INA333 in a PT100 reader circuit and only need good performance near DC. Is it possible to limit the gain bandwidth of the INA333?
Hey Adam,
Since the INA333 is a closed-loop device, there isn't really a way to directly limit the BW of the device. Technically, increasing the gain will lower the 3dB bandwidth, but this does not change the UGBW of the device. What benefit are you looking to realize by lowering the GBW? Increased noise performance?
Best,
Gerasimos
Hi Gerasimos,
Yes that is correct. If i have some noise on the RTD cables, etc.. then it would be better if this were not gain'ed up.
In the absence of a way to limit the BW, then also given the high input impedance and low bias current requirements of the INA333 I can instead put some common mode filtering at the input. Maybe 10K on each input and 1 uF between them?