Part Number: LM13700
Tool/software:
I have attached a TINA simulation of LM13700 in which I want to limit the output voltage. Please consider the following requirements
1. When I am giving an input of 383mV peak to the amplifier the limiter IC should not come into action.
2. When the input is greater than 383mV the limiter should come into action and limit the output to 700mV.
3. I have used a PNP transistor to turn on and give the drive current to the limiter.
4. I am not getting any change in the output .. Why?