This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9001: TLV9001

Part Number: TLV9001


Tool/software:

Hi,

I would like to connect speaker as microphone , and i will need to connect op amp in differential connection with 24dB gain, please note that the speaker also connected in parallel  to the audio PA that generate 30Vrms with 400Wrms , so i can have scenario that the audio PA will drive the speaker and i will have on the op amp input 30vrms.

Could you recommend how can i protect the inputs of the TLV9001, please note that i will use a single supply 5V for the Op amp 

Thanks Hadi