Other Parts Discussed in Thread: OPA192, OPA197
Tool/software:
Hello,
I have some question regarding the shutdown function of the TLV9151S that mean TLV9151 with Shutdown function.
I'm not sure I understand everything so:
- The TLV9151 is defined as mux freindly on the website page, but not in the datasheet, It is mux friendly ?
- If yes, is the "Mux friendly" is The TLV9151 similar to the description present in the TLV9351S datasheet ?
- More practically In the case of a simple negative feedback assembly with the TLV9151S what will happen to the IC when 16V is applied to Vout when shutdown enabled ? What will Happen to IN + ?
- What will happen if the IC is not powered but grounded when 16V applied to Vout ?
- The "7.4 Device Functional Modes" introduce me a doubt about working supply range, it's 16V or (+/- 8V) ?
Thank-you for support !