This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH5401: LMH5401: Output Vcm adjustable circuit

Part Number: LMH5401
Other Parts Discussed in Thread: LMV771

Tool/software:

Hi:

I hope to use LMH5401 to design a circuit with adjustable VCM output.
The working voltage of LMH5401 : VCC = 3.15V , VEE = -2.14V
It is hoped that the VCM output will be in the following range: [-500mV  500mV]
Single ended output voltage swing: 1 Vpp

I tried to simulate it with TINA, and the function was OK.

I wonder if the actual operation of the circuit will be consistent with the simulation.

Hope experts give advice!
Thanks!

LMH5401_20250121.TSC