Part Number: INA239
Tool/software:
Hii,
we are using INA239 for our project, following are the specs.
Current Measure : 450A
Rshunt : 100uOhm
following are some queries
1. If we are not using VBUS pin ,can it be left floating
2. The INA239 freezes if we measure current more than 50A
3. The shunt is busbar type ,the distance betwwen INA239 and shunt is more than 20cm how can mitigate the effect of harness drop,will extra filter helpful
4. we are powering INA239 using 3.3V is that effect the IC performance
Regards
Mudit Mittal