Part Number: OPA593
Tool/software:
Hi,
I am using an OPA593 as a buffer (unity gain).
The op.amp. is not oscillating. , however I observed a high current consumption (more than 50mA from 60V) even with the input connected to GND.
Any idea why?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA593
Tool/software:
Hi,
I am using an OPA593 as a buffer (unity gain).
The op.amp. is not oscillating. , however I observed a high current consumption (more than 50mA from 60V) even with the input connected to GND.
Any idea why?
Hello Cezar,
Could you please post a schematic? If not, please specify what type of loads are connected to the output and the power supplies? Is it 60V single-supply or dual-supply (±30V or some variation that adds to a voltage differential of 60V)?
Here is what is expected:

At the following conditions:

All the best,
Carolina
It is a single 60V and no output load.
I know that it is away more than expected.
I can share the schematics, but not in a public forum. Can you share somehow your ti.com email address?
Hey Cezar,
This is abnormal for the OPA593.
I am working with a TI FAE on this problem you are seeing. Sachith (TI FAE) shared the current schematic with me.
Can you tell me the output voltage of the buffer when you are connecting the IN+ to GND?
When you measure the 50mA, is this with U4 removed, or with U4?
Thanks,
Jacob