Part Number: LOG200EVM
Other Parts Discussed in Thread: LOG200
Tool/software:
Hi PSC team,
Company x needs to measure very low currents into the pA, for that they are evaluating the LOG200EVM and have some questions, could you please have a look at them?
Now I have some questions about the internal (1uA) current-source of the EVM.
They need to measure very low currents down to 1pA (there they can have a bigger tolerance). For that they should go in to the board with a lower current on I2 (for example 100pA).
Should they put the 100pA with an external source, or can they use the 1uA current-source and make the 100pA with that?
If they have on the VCM node, the REF25, is it also possible to have a load resistor on the I2 to GND and then a part of the source current flows into that path?
![]()
![]()
Thank you.
Kind regards,
Wouter Kragt