Other Parts Discussed in Thread: OPA859
Tool/software:
Hello team,
I see OPA3S2859 can be used with >100kΩ gain resistor.
Is there any maximum gain resistor value?
OR can we use like 1MΩ?
Best Regards,
Kei Kuwahara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kei,
I am looking into it. Can you clarify one thing please: Are you planning to use this as a voltage in voltage out opamp or as a TIA with a photodiode?
Regards
Aditya
Hi Kuwahara,
Considering OPA3S2859 is built on top of a high-speed op-amp (presumably OPA859), you can use higher gain resistors like 1MΩ. However do keep in mind with higher gain resistors, there will be tradeoffs such as slower settling time, lower slew rate and prone to noise and output voltage offsets (due to resistor rating and input bias, which is minimal in this case, 50pA * 1M = 50uV).
Regards,
Adam Zahanuddin
Hello Aditya-san, Adam-san,
Customer is going to use this OPA3S2859 for I/V conversion, but input is not photodiode.
Its more like current sensing application.
So, there is no max gain resistor limit?
Is so, then what are the differences between Low gain, Mid gain, High gain FB path?

Best Regards,
Kei Kuwahara
Hi Kuwahara-san,
I have attached a similar query below, where difference between the 3 channels is explained in detail.
For the max Rf limit, I think Adam has explained it very well. If you want to check the effect of Rf (or any other input parameter) on output parameters like: settling time, noise, offset error, etc. The value of Rf resistor also decides the stability of the OpAmp, as Rf and inverting input capacitance of the OpAmp will form a pole in feedback loop. Higher the value of Rf, the OpAmp is closer to instability.
Please have a look at our TIA tool as well as current sensing tool: Analog circuit design studio where you can insert all the input parameters as per your need and check the output parameters accordingly.
Please try out the tool and let me know what do you think.
Another query regarding the same question of difference between 3 channels: https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1219902/opa3s2859-ep-opa3s2859-ep-clarification-for-datasheet-specs
Regards,
Aditya
Hi Aditya-san,
Thank you for your answer!
I understood now.
Best Regards,
Kei Kuwahara