Part Number: INA4180
Other Parts Discussed in Thread: AM3358
Tool/software:
We are using the INA4180A1IPWR sense amplifier with a 0.001 ohm current sense resistor. We're attempting to measure between 6 and 7 amps of current through the .001 ohm resistor. That produces between 6 mV and 7 mV at the input of the sense amplifier. Is this level of voltage too low for accurate current measurement? Are there noise issues? We are seeing about 180 to 190 mV at the output which is indicating too high (should be seeing 120 mV to 140 mV).