Other Parts Discussed in Thread: TAS5412-Q1
Tool/software:
Hi expert,
Our customer want to use H bridge driver for buzzer under following requirement:
・H bridge IC (Automotive)
・Analog Input, Output(PWM) x2
・Input voltage:Max 5.15V
・Output current:Max 950mA
・Signal frequency:20Hz~20KHz
・ Speaker Impedance:8ohm
・They prefer short transition delay between Forward/Reverse
I would like to recommend customer TPA31102D2-Q1 or TAS5412-Q1 but those are little higher output power.
Do we have any candidate for this opportunity?
Best Regards,
Yusuke