This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM360: thermal resistance

Part Number: LM360
Other Parts Discussed in Thread: TL3016, TL3116, TLV3601, TLV3501

Tool/software:

hello team
can you provide the thermal resistance values for the LM360MX/NOPBR?
  • Hello Kodama,

    I could not find any thermals on the SOIC package.

    I can put in a request, but be aware that it may take a week or two to get the results.

  • Hello paul,

    I would like to request information regarding thermal resistance. Additionally, could you recommend a product with similar functionality to the LM360? In an older thread, the TL3016 was suggested; is that still correct?

    https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/779357/lm360-lm360-operation-temperature-range/2882270#2882270

    Best Regards,

    kodama

  • Hello Kodama,

    There is also the TL3116, which has an input that can extend down to V-.

    What are the main needs for your design? Speed? Supply voltage? What is the application?

    What are your input signal levels and speed, available supply voltages, and output swing requirements?

    These are older devices and their are many newer devices, especially under 5V.

  • Hello paul,

    I was selecting the LM360 as an alternative to the NJM360M (Nisshinbo), but I inquired about the thermal resistance due to the possibility of it conflicting with the operating temperature. If the thermal resistance indicates that the operating temperature is acceptable, I would like to use the LM360.

    The required comparator input/output specifications are as follows:

    • Supply: V+ = +5V, V- = -5V
    • +IN: AC -0.3V to 1.5V
    • -IN: DC 0.4V
    • OUT: AC 0 to 5V; inverting output is required
    • Speed: Equivalent to LM360MX/NOPB; this is important as it may affect the latching of the FF in the output circuit block.
    • Operating temperature range: Above 85℃
  • Hello Kodama,

    Here are the thermal results for the LM360MX/NOPB

    Theta JA-High K:

    123.1

    Theta JC, top:

    60.3

    Theta JB:

    71.1

    Psi JT:

    7.9

    Psi JB:

    70.1

    Theta JC, bottom:

    n/a

    Do you need the differential outputs? Could you use LVDS? What are your logic levels?

    Unfortunately, most of the "fast" (<20ns) devices are 5V maximum.

    If you run off a single supply, then there are more options, such as the TLV3501 or TLV3601 family.

  • Hallo, Paul
    Thank you for providing the thermal resistance information. Unfortunately, due to the lack of margin for the operating temperature, I have decided to select an alternative product.

    I would like to correct the input, as it was previously inaccurate. The correct value is +IN: AC -1.2V to 1.5V. The output specification requires complementary outputs. I will first conduct a verification of the current circuit to determine whether either the TL3016 or TL3116 can serve as a suitable alternative.

    Best Regards,
    kodama