Part Number: AMC1200
Tool/software:
Hi
i am using a acm1200 device to monitor a supply voltage. All is well at ambient, but below -20 get errors (dips) even though the supply is driven from a PSU.
as this a controlling a motor, noise may be the issue. the circuit is similar to the datasheet but optional diff filter caps are not there.

also c2 is 100n and r2 and r3 are 39r. Rshunt is 60R. vdd1 is 5V and vdd2 is 3.3v supplied by own regs, so no zener is required. The output is fed to a diff amp with a gain before being feed to the adc.
I am going to add the C3 and C4 caps (1uF). how import is the filter do i need to reduce any values in resistors and caps?
regards
Ross