Part Number: TLC2272
Other Parts Discussed in Thread: TLV2186, OPA2186, INA180, TLV2888
Tool/software:
Hi,
I'm looking for a reason of this issue:
- I have the follow circuit to sense the current (shunt + OpAmp)

- The OpAmp is a MCP6002 of Microchip
- When there is no current flowing through the shunt R234 and R241, the voltage level on pin 1 of OpAmp is 0.06V and 0.6V on pin 7 of OpAmp.
- If I use the TLC2272 instead of MCP6002 these levels of voltage are near 0V.
Why does the output voltage of the MCP6002 deviate from 0V
Best regards,
Andrea