This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV3202: TLV3202

Part Number: TLV3202

Tool/software:

Hello,

We are planning to use the TLV3202AID comparator in one of our projects.

Requirements:

  • Input Range: 600mV to 3V (Pulse Width : 10uS to 200uS)
  • Output Range: Dynamic

Test Observations:

Circuit:

  1. Result 1:

    • Input Signal (Function Generator):
      • Frequency: 100 kHz
      • Duty Cycle: 50%
    • Observation: The output is correct.
  2. Result 2:

    • Input Signal (Function Generator):
      • Frequency: 1 kHz
      • Duty Cycle: 50%
    • Observation: Noise is present in the output.

Please review the attached circuit and test results and let us know what needs to change in the circuit to achieve our requirement.

Looking forward to your feedback.

Best Regards,

Kruti Panchasara