Part Number: OPA858
Other Parts Discussed in Thread: TINA-TI
Tool/software:
Title: Stability of OPA858 in Transimpedance Amplifier (TIA) Configuration
Question:
I am working with the OPA858 op-amp and trying to use it in a Transimpedance Amplifier (TIA) configuration. From the datasheet, I see that the op-amp is decompensated with a gain bandwidth product requiring a minimum gain of >7 V/V for stable operation in a voltage amplifier configuration.
In the voltage amplifier case, the gain can be stabilized by setting the resistor values such that R2=7R1R_2 = 7R_1R2=7R1. However, in the TIA configuration, there is only a feedback resistor RfR_fRf, and the input is a current source with infinite impedance. Given this, my concern is:
- Since there is no explicit gain-setting resistor like R1R_1R1 and R2R_2R2 in a standard amplifier circuit, how do we ensure that the OPA858 remains stable in a TIA configuration?
- Does the feedback resistor RfR_fRf alone determine the stability, and if so, how do we calculate a stable value?
- The datasheet mentions TIA applications, but doesn't the infinite input impedance from the current source make the op-amp unstable?
- Can I use the OPA858 as a TIA without additional compensation, or do I need to add external compensation components?