Other Parts Discussed in Thread: OPA593, OPA593EVM, ALM2402Q1EVM, ALM2403-Q1
Tool/software:
We are looking for a solution to increase the driving signal sources 0 to 10v (with resolution 0.01 steps) from 4mA to 80mA. So, the output signal should look like the same with input signal voltage but in 80mA.
i.e.
input signals : [0 -10V] , 4mA
Required Out Signal : [0-10V]linear , 80mA
Basically an linear voltage with current amplified up to 80mA .
Kindly check and help with this.