Part Number: UCC28740
Tool/software:
Hi,
Please help to check our schematic and there are no 12V output voltage for our design:
We have below issue:
1. The VDD waveform(Yellow line) and DRV waveform(Blue line), is it right?

2. We want the input voltage is 90-260VAC and output voltage is 12VDC, and the Npa is 5.5, the RS1 is less than Vin(run)=90, Is it right?

3. The schematic diagram refer to below: