Part Number: TLV9002-Q1
Other Parts Discussed in Thread: TLV3231, TLV3201, TLV9031
Tool/software:
Hi,
My customer is designing a 48V auto BMS system. orignial, they are evaluting TPS4800 + INA solution to meet bi-directional low side OC detection, but due to cost sensitive, I'm reommending TPS4800+ ampliger solution, 4800 could detect OC on discharing direction, amplifer circuit do the other direction OC detection.
so, would like to check if low cost Q-grade Amplifers could do this, do you have PN and design recommendation?
BTW, the output of OC signal need to directly control TPS4800 to open and close contactor. thanks.
SPEC is as below:
1. 10A accuracy 1%
2. power consumption : 0.1mA max