Part Number: INA254
Tool/software:
Hi,
I have using INA254A2 to run a test. The gain written inside the datasheet for INA254A2 is 40 mV/A .
I have changed the position of R203 to R204 to enable my Ref1 and Ref2 are both connected to ground. Besides, I am lifting up the pin 10 to input a -2.5 V in to activate the board together with +2.5 V in the VS.
Here comes the situation
When I input a 30 A to the IS+ and IS - , it gives me the output of 1.5 V, which supposing I should get 1.2 V.
Based on theoretical calculation:
Vout = I X Gain
Vout = 30 A X 40 mV/A
Vout = 1.2 V
Can I get an explanation on this issue?
Thank you
Regards,
Willie