Part Number: LM5148
Tool/software:
Hello,
When the LM5148 is in PFM modulation, does it always use the min on time, or modulate that?
Thank you, Keith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5148
Tool/software:
Hello,
When the LM5148 is in PFM modulation, does it always use the min on time, or modulate that?
Thank you, Keith
Hello Keith,
No, the on time is set by the Peak current limit in PFM mode. Where the PFM peak current limit is 20% of full scale current limit. Hope this makes sense.
David.
Hello David,
Could you please help me with the math?
Vin = 36V
Vout = 3 - 21V
Iout Max = 8A
switching freq 220kHz
inductor 8.2uH
What is the maximum peak inductor current we could expect with 20% output, so 1.6A (8A x 0.2)?
Thank you, Keith