Part Number: LMH6503
Other Parts Discussed in Thread: LM27762, THS4541
Tool/software:
Hi Sir,
The customer found the LMH6503 IC will get hot after power on with no input signal!
The power supply provides 4.3V as a power source for LMH6503 and boosts IC(LM27762). The current consumption is 60mA, as shown on the power supply.
The LMH6503 temp. will increase around 7~8 degreeC and boost IC temp. increase around 5 degreeC after 2mins later.
Wait for the system to stabilize and measure the AGC output(red circle) and the waveform as attached.


The increased temp. will narrow the pulse width to around 6ns.
Please help to check if there is anything wrong with the design and any advice is appreciated!
Thanks.