Tool/software:
Dear Team,
My customer has questions about the Current Limit Set pin of the OPA569.
Q1: When the Current Limit Set pin (3-pin) is opened, what is the current limit value? 2.2A or o,2A?
Q2: Behavior when the Current Limit Set pin (3-pin) is conneceted to V+ instead of V-.
With the maximum rating of 3-pin, the voltage range is from (V-) - 0.5V to (V+) + 0.5V, so there is no fatal damae, right?
Best Regards,
Koshi Ninomiya