Part Number: OPA322
Other Parts Discussed in Thread: TINA-TI
Tool/software:
Hello team,
Does the spice model have parameters for capacitive loads? (simulate vs capacitive loads?) My customer thinks to use ~10nF load.
Best regards,
Shotaro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shotaro,
Yes, our macro-models are specifically designed to model stability of the circuit - please review following link:
https://www.ti.com/video/series/precision-labs/ti-precision-labs-op-amps.html
The circuit stability with the capacitive load is a function of circuit configuration like gain and is typically shown in graph in terms of the small-signal overshoot - see below.

In order to assure stability over process and temperature variation, it is recommended to design the circuit for the maximum overshoot of 25%, which corresponds to 45 degrees phase margin. Simulating OPA322 driving directly (no Riso) 10nF load shows only 3 degrees phase margin - see below.

The marginal stability of OPA322 in G=1 may be confirmed by running transient simulation - this shows a small-signal overshoot of around 100% overshoot - see below.

In order to assure stable operation with recommended 45 degrees phase margin, it is necessary to add outside the close-loop 7ohom Riso resistor as shown below.

Transient simulation confirms stable operation with a small-signal overshoot of 19% - see below.

For your customer's convenience I have attached below Tina-TI simulation files for OPA322.
Your customer may download a free version of Tina-TI PSpice simulator by clicking on the following link: https://www.ti.com/tool/TINA-TI