Part Number: PGA309
Tool/software:
I'm planning on implementing temperature sensing and bridge excitation per this schematic. This will allow my bridge common mode voltage to remain roughly centered about VEXC/2 so that I can take advantage of the input PGA's high gain (128) while taking into account the Coarse Offset DAC's limited range (~±60 mV). I would connect Temp+ to the TEMPIN input and use VEXC for both the Temp ADC Input Mux and Temp ADC Reference. Looking at figure 2-20 of the User's Guide (Rev C), it appears that the Temp PGA gain is performed after the differential voltage is determined. I.e., with a gain of 8x, it seems OK with 2.747V and 2.9V at the Temp PGA inputs. I want to confirm if this is accurate or if I would need to use an external difference amp and lower the common-mode temperature voltage closer to ground.