This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA326: I need same functionality IC but operating temperature range with -40°C ~ 125°C

Part Number: INA326


Tool/software:

INA326 for this operating temperature range is -40°C ~ 85°C  but my requirement is we need to use under the 110°C can you suggest the alternate part

  • Hi Manohar, 

    Welcome to E2E! 

    The INA326 can operate up to +125C; we do not provide specifications in the datasheet for that range, so parameters may vary at 110C. 

    This part has a unique architecture and pinout, so we do not have other pin-to-pin alternatives. If you can provide some details of your application needs, we can look into similar parts that can fit your need. 

    Regards,
    Ashley

  • Thank you for information .


    can you suggest any reference design or IC for 2 wire PT1000 RTD using instrumentational amplifier.

  • Hi Manohar, 

    What are your device requirements for the instrumentation amplifier? Such as power supply, package, level of precision, what load you are driving, etc? 

    Regards,
    Ashley