Part Number: TLV369
Tool/software:
Hi
Could you help recommend a high bandwidth OPAMP, Hopefully the slew rate can be around 5V/ns
Vin =12v
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Gareth.
Do mean 5V/ns = 5000V/uS? That a million times faster than TLV369.
Gareth,
What is the amplitude range of the 10MHz input sine? Is the question for signal conditioning, decoding, or both?
input decoding
What aspect of the input becomes the output? In other words, how should the decoding work.
Gareth,
You need a comparator and a fast one. How fast, depends on close in phase the zero cross should happen at output.
If phase doesn't matter as long as output has fast edges then it won't need to be as fast.
Fast comparators are here. https://www.ti.com/amplifier-circuit/comparators/products.html#83=0.005%3B0.099&