Part Number: UA741
Other Parts Discussed in Thread: TLE2021, TL071, OPA277, OPA177, TL031
Tool/software:
Hello, we have bought a bunch of op-amps UA741CP from Mouser distributor and tried to use them in one of our typical data acquisition and control boards but have found the input offset pins are not working since we cannot compensate the input offset (actually the output is not changing at all by operating on R11 trimmer). We are testing it with R1 and R2 connected together, so zero volt input.
The offending parts are marked 48AELYM-G4
This is an abstract of the electrical drawing showing a typical circuit in which the op-amp is used (we are using this kind of circuit extensively in several boards of our production):

We have checked board circuitry and found nothing wrong, moreover using other 741s we have in our lab the offset circuit is correctly working on the very same board.
We have checked 10 out of 100 pieces bought and found all defective. This is an image of components not working correctly:

An example of 741 correctly working in the same board is marked differently (01AK7DM).
What can be the problem here? It seems this lot of components is not working correctly.