Part Number: USB2ANY
Other Parts Discussed in Thread: LMP92066, , LMP92066EVM, MSP430F5529
Tool/software:
Trying to use the USB2ANY with LMP92066 bias controller. Seems to have a lot of bugs... but was working through that and realized that the I2C lines in the USB2ANY are pulled up too high. OUr target LMP9266 is on 1.8V I2C bus. The USB2ANY manual says that pullups can be disabled but offers no help on how to do that.
Related question - the USB2ANY seems to imply that the I2C levels must be 3.3V. Is that true? In that case, will I be able to program my LMP9266 on a 1.8V I2C bus without isolating the IC from the bus on the board?
To be clear, the LMP92066 is on a final target board. There are no masters on the bus (sort of, there is a multimode master so it should not be interfering).
Quick resolution is appreciated. We are on a time crunch.
Thanks in adavance.