Tool/software:
Hi,
I need a differential to single-ended converter. The input signal has 1MHz bandwidth and a Vcm=1.65V, Vmax 3V, Vmin 0.5V.
The output is connected to an ADC of a uC, power supply 3.3V.
Thanks for support.
Best Regards
Hello,
Is the power supply a single power supply rail of 3.3V? So the INA would be connected to 3.3V and ground?
And will you be setting the gain to 1?
Regards,
Ashley
Hello HD,
I would recommend trying the INA823 (INA823 data sheet, product information and support | TI.com) based on your requirements listed above.
Please let me know if you have any questions.
Thank you!
Regards,
Ashley
Hello Ashley,
ok thanks for information.
In the meantime I had also found the same product you suggested.
It seems a good product but it is the only IC in the TI catalog that meets all the requirements. I also tried to see possible alternatives from other manufacturers without success. At this point I have to ask you... is it possible to know the life cycle of this product? How long will it still be produced, just to make some future predictions.
Kind regards
Hi HD,
Good to hear - please let us know if you have any questions on implementation or other application questions on the INA823 and we would be happy to help!
Product life cycles at TI are generally 10-15 years and often longer and our product page will have the most up-to-date information on the current status of the product.
Please see our policies on product life cycle here: Product life cycle | Quality policies & procedures | TI.com
Regards,
Ashley