Other Parts Discussed in Thread: LMH6628, , LMH5401, LMH6654, LMH6702, LMH6639
Tool/software:
Hi TI-Team,
we have a radiation (SET) issue with LMH6628 in an analysis. Therefore, we are searching for a solution. We try to simulate the transient and the effects on the following circuit/parts. We recognized that there were examined other LMH components. Another solution for our analysis could be a compare to other devices with the same technology. Also, it would help to know the SET pulse time (actually we have to use a worst case approach from ECSS-Q-ST-60-15C with pulse time of 15us).
Q1: What is the die size of the LMH6628QML-SP? Can you characterize the ASET cross-section for that device?
Q2: Can you confirm that the LMH6628QML-SP is produced with the VIP-10 process?
Q3: We have SET test data for LMH6639, LMH6654, LMH5401 and LMH6702. Which one is most comparable to the LMH6628 (die size, functionality, production process, etc.)
Q4: The maximum SET pulse time within the SET test data is <10ns. Could it be assumed that the SET pulse time for the LMH6628 is similiar?
Test data is available here:
https://radhome.gsfc.nasa.gov/radhome/papers/L061806_LMH6702.pdf
Best regards, Alessandro