Part Number: TLV1872
Other Parts Discussed in Thread: DAC61416
Tool/software:
Hi team,
My customer uses DAC61416 to set the reference voltage of DUT and feed into inverting input (IN-) of TLV1872. The supply condition as follow:
- VCCI=24.5V.
- VEEI=-13V.
- The positive & negative supply voltages are shared between DAC and comparator.
Because DAC61416 has a short-circuit current of 40mA, could you help to evaluate:
- Do we need to place series current limiting resistors (RINs) at the inputs of TLV1872? If so, what is the recommended resistor value?
- Do we need to place same RINs at both IN+ & IN- ports?
Thanks,
Frank