This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA700: Multiple device sampling synchronization

Part Number: INA700

Tool/software:

Is there a way to synchronize multiple of these devices such that they perform conversions in parallel (e.g. a broadcast command for triggering)?

  • Hello Steve,

    While we don't have a direct synchronization pin, you can try to align measurements using triggered conversions and the conversion delay (CONVDLY) feature. For example, if you are trying to synchronize 2 devices, then you can set one device to convert after 10ms, then after 5ms you can tell the second device to convert after 5ms. This way they both start conversions around the same time.

    Regards,

    Mitch