Part Number: INA226-Q1
Tool/software:
Dear teams,
INA226-Q1 Shunt voltage input range ±81.92mV,
for example when using shunt resistor 0.1mΩ, measure current up to about 800A, is it right?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chu,
Yes, you can measure up to 800A, but please note that your 0.1m shunt resistor must then also be able to dissipate I2R power.
Best,
Mallika Senthil