Part Number: OPA333-Q1
Other Parts Discussed in Thread: OPA333
Tool/software:
Hello,
This is Akhil. I am currently working on a speaker-related circuit and require support in designing a 5V, 1A DC converter from the output of an audio amplifier. The audio signal frequency is 20 kHz, and the amplitude is 15V, with the current approximately reaching 4A. Could you kindly provide any suggestions or a suitable circuit for this application?