Other Parts Discussed in Thread: INA118, INA111, INA110, INA166, INA163, THS4221, INA826, INA331, OPA365
I would like to use an instrumentation amplifier to amplify a strain gauge bridge signal (on the order of mV) to an amplitude of V (a gain of 1000). The voltage signal I would like to amplify is actually a square pulse which goes from 0 mV to approximately 5 mV and back to 0 mV over a time span of approximately 30 micro-seconds (a strain pulse from a Split Hopkinson Pressure Bar experiment). The instrumentation amplifier has to meet the following two conditions:
1. Be able to be powered by a positive DC voltage from a constant power supply source (I can easily manipulate this supply voltage to whatever is necessary).
2. Be able to accurately amplify the very rapidly rising and falling square pulse of the input signal.
A colleague suggested using the instrumentation amplifier INA118. Will this component meet my needs?
Thanks,
Nathan