This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLE2037: TLE2037CD Performance problem

Part Number: TLE2037

Tool/software:

 Hi

This product, we use on the computer found that there is an anomaly, after replacing one is OK
Could you please help confirm the cause
Thank you

  • Hi Yingjiao, 

    This product, we use on the computer found that there is an anomaly, after replacing one is OK

    I need more information about your Pass/Fail criteria. 

    These parts are older lot, For instance, 71M refers to 2017 date code and 13M is dated 2001. TLE2037C, where C is lower grade, AC is higher grade - meaning lower Vio. 

    Could you send me a schematic and tell me how you screen OK and "NG"?

    If you have other questions, please let me know. 

    Best,

    Raymond

  • Hi

    1. How does VIO test?
    2. When SH+ and SH- are short-circuited, pin 6 of U8 still has a voltage output of 2.4mV. What is the reason for this
    3. Working voltage supplied to TLE2037CD(U8) : +VA=12V, -VA=-12V

  • Hi Yingjiao, 

    1. How does VIO test?
    2. When SH+ and SH- are short-circuited, pin 6 of U8 still has a voltage output of 2.4mV. What is the reason for this

    The table below is the Vos voltage  refers to the input, which is a buffer configuration. 

    Your difference amplifier has a gain of 65.934V/V, and your output offset voltage is up to 100uV*65.934V = 6.59mV_max, and you measured at approx. 2.54mV, which is expected (Vio*gain) between typical (25uV*65.934 = 1.648mV) to 6.59mV due to the op amp configuration alone.   

    This Vio voltage specification is only a part of dominated offset voltage errors.  The overall offset errors are shown in the equation below and you are well  below the max. possible errors in this part. If you use TLE2037AC grade, your overall offset errors will be smaller, but it is still there. 

    Here is our precision op amp video series in the Vos topics. Please check it out. 

    https://www.ti.com/video/series/precision-labs/ti-precision-labs-op-amps.html?keyMatch=ti%20precision%20lab%20series&tisearch=universal_search

    If you have other questions, please let me know. 

    Best,

    Raymond